Program
   BeforeStart
     Move to Initial start position
       MoveJ
         'CAUTION: check reachability or edit Waypoint before running Demo!'
         Start
     FT Sensor: Enabled
     'Initialize variable for use in Thread:'
     'In this example, we name the variable ATI_FT_data.'
     ATI_FT_rawdata≔ati_ftsensor.get_raw_ft()
   Robot Program
     Bias the sensor
       Wait: 0.5
       FT Sensor: Bias
       Wait: 0.5
     'This Demo program shows multiple ways to search & monitor forces (without UR Force Mode)'
     'and program offset motion with UR Force Mode.'
     METHOD 1
       Move down until the tool touches a surface
         'Monitor Norm of Forces (in robot base coordinate frame)'
         MoveL
           If ForceNorm<2
             RelativeMotionZ
       Move across the surface while applying 10N of force
         'Use "Simple" type UR Force Control'
         Force
           MoveL
             Wait: 1.0
             (Optional IF) Stop if the tool encounters too much resistance or hits wall.
               If xyPlaneForce < 10
                 RelativeMotionX
         Reset to a start position
           MoveL
             Up
             Start
     Reset to a start position
       MoveL
         Start
     METHOD 2
       Move down until the tool touches a surface
         'Monitor Norm of Forces (in robot base coordinate frame)'
         MoveL
           If ForceNorm<2
             RelativeMotionZ
       Move across the surface while applying 10N of force
         'Use "Motion" type UR Force Control with only Z compliance'
         Force
           MoveL
             Wait: 1.0
             (Optional IF) Stop if the tool encounters too much resistance or hits wall.
               If xyPlaneForce < 10
                 RelativeMotionX
         Reset to a start position
           MoveL
             Up
             Start
     Reset to a start position
       MoveL
         Start
     METHOD 3
       Move down until the tool touches a surface
         'Monitor Norm of Forces (in robot base coordinate frame)'
         MoveL
           If ForceNorm<2
             RelativeMotionZ
       Move across the surface while applying 10N of down force & 0N of side force
         'Use "Motion" type UR Force Control with Y & Z compliance, only push in Z'
         Force
           MoveL
             Wait: 1.0
             (Optional IF) Stop if the tool encounters too much resistance or hits wall.
               If xyPlaneForce < 10
                 RelativeMotionX
         Reset to a start position
           MoveL
             Up
             Start
     Reset to a start position
       MoveL
         Start
     METHOD 4
       Move down until the tool touches a surface
         'Monitor raw FT sensor readings (in sensor coordinate frame)'
         MoveL
           If ATI_FT_Fz>-2
             RelativeMotionZ
         Wait: 2.0
       '(Optional) Insert a UR Force Mode command to move across the surface, as shown in Methods above.'
       Reset to a start position
         MoveL
           Up
           Start
   Thread_1
     'MONITOR THIS DATA DURING PROGRAM FROM "Variables" TAB'
     Wait: 0.01
     'Read sensor F/T Data using F/T URCap command, & assign it to a variable.'
     'This is the raw data directly from the sensor, in the sensor coordinate frame.'
     'With every loop of the thread, update the raw F/T data reading.'
     ATI_FT_rawdata≔ati_ftsensor.get_raw_ft()
     'Fz is the 3rd element of the ATI_FT_data variable.'
     'NOTE: Pressing sensor in Z causes a -Z force (if no sensor Tool Transform applied)'
     ATI_FT_Fz≔ATI_FT_rawdata[2]
     'F/T sensor data can also be read from native UR commands.'
     'Data read from UR commands will have transformations applied.'
     '(it is in robot base frame, not in the sensor coordinate frame).'
     ' UR Command get_tcp_force() gives TCP force in coordinate frame of robot base.'
     FTinBaseFrame≔get_tcp_force()
     'UR command force() gives the Norm of get_tcp_force().'
     ForceNorm≔force()
     Get magnitude of force in just the X-Y plane, accounting for friction of tool
       xyPlaneForce≔sqrt(pow(FTinBaseFrame[0], 2) + pow(FTinBaseFrame[1], 2)) - 0.3*ForceNorm